2021-02-07 9:26 PM
Hello,
I am using L9663 PSI5 transceiver for the development of a steering drive project. I have a doubt regarding the SPI communication. If I want to read a register content will I be able to get it in the same MISO data?
For example, I am sending a 32-bit SPI data (MOSI) to read the content in register "SR1". Can I get the data in the received SPI frame (MISO)?
Please clarify.
Best Regards
Varun R
2022-08-31 8:40 AM
Yes, this is the design of the SPI protocal to have a replsonse from MISO in the same transfer.