2025-05-13 11:47 AM
I am trying to communicate with an external flash chip “MX35LF1G24AD” using QSPI protocol, but I am not able to.
Simple test I implemented was to read chip ID to validate I could get data from external flash (I am using OCTOSPI1 interface).
From manufacturer datasheet it is mentioned that command should be sent using 1 line on SDIO0. However, when probing communication, data is sent from SDIO3.
Is it possible to send command, on 1 line, on SDIO0 pin instead of SDIO3?
2025-05-13 12:11 PM
>>Is it possible to send command, on 1 line, on SDIO0 pin instead of SDIO3?
Sounds like you've not configured the command structure correctly.
https://www.macronix.com/Lists/Datasheet/Attachments/9034/MX35LF1G24AD,%203V,%201Gb,%20v1.4.pdf