2024-09-10 8:29 AM
In AN5041 Rev 5, pages 26-28, there is an example programming sequence for the STEVAL-IDP004V2 master and a device on a STEVAL-IDP003V1 using ST's customized protocol (a substitute for IO-LINK).
Is there a manual or tutorial or resource page that goes through programming the boards and communicating with them with ST's customized protocol?
2024-09-10 9:27 AM
Hello,
Check out this video and see if you find what you are looking for.
2024-09-11 11:27 AM
Thank you SofLit, I have that other kit as well, the documentation is more clear to me too.
I still have the issue of what to do with my 4-port master hub since it has been programmed with the ST Customized Protocol, see AN5041 - Rev 5 page 22. I programmed the STEVAL-IDP004V2 hub with the file "STEVAL-IDP004V2-RS485.hex". It seems for this setup with the STEVAL-IDP003V1, the IO-Link demo is the simpler way, but, after much searching, where is the hex file for programming the STEVAL-IDP004V2 (AN5041 - Rev 5, section 5 on page 29)? Notice how the documentation's steps don't say what the hex file is and where to get it from. I can't find it on ST's site, there only seems to be IO-Link libraries, but no hex file to set the board back to what it was from the factory. Once that is done, then I can try the video you mentioned with the IO-Link Master example.
Where do I get the hex file for the IO-Link setup for the STEVAL-IDP004V2 hub?
What is the process to renew the license?
Thank you,
-James