cancel
Showing results for 
Search instead for 
Did you mean: 

LIV3F's input Vcc_io gets randomly tied to gnd

ABouk.1
Associate III

Hi everybody,

I have been using for a while liv3f product and, before creating the schematics i read carefully the hardware manual and the electrical caracteristics.

Once I have put it on a pcb, it was working well and i was getting gps signals. But after no more than 4 days, the input Vcc_io becomes tied to Gnd and the module does not work anymore.

This problem have been happening for 3 times now, I am really confused because I don't know why.

The LIV3F pins are connected as follow :

  • TX -> MCU RX
  • RX -> MCU TX
  • 1PPS -> MCU input
  • WAKE-UP -> MCU output
  • VCC_IO -> 3v3
  • VCC -> 2v4
  • SYS_RSTN -> MCU output (usually 1)
  • VCC_RF -> not connected
  • ANT_OFF -> not connected
  • RF_IN --- 100 nH Inductor --- 3v3 ---- 120 pF capacitor ---- GND (connected to external active antenna)

0 REPLIES 0