cancel
Showing results for 
Search instead for 
Did you mean: 

STHV748 Technical Support

hwijinkim
Associate

Dear Manager.

Hello, I am a student studying at a Korean university.

I am developing a two-channel small ultrasound system.

1. Try to use STHV748, a 4-channel pulser, as a pulsar, and don't use the other 2 channels. Should I connect to GND for channels I'm not currently using?

2. If I want to use it as a three-levels pulser instead of a five-level pulser, should I supply the same high voltage to HVP0_X and HVP1_X? Or should I connect HVP1_X to GND?

Thank you. 

From hwijin.

0 REPLIES 0