cancel
Showing results for 
Search instead for 
Did you mean: 

Image file httpfsupdate maximum size

paulcatherall9
Associate II
Posted on September 02, 2016 at 17:02

Hello

I am using a Nucleo F103 RB with XNUCLEO-IDW01M1

 board to develop the code.

I have been successfully using the Update over the air feature for some time.

I now have an image file that has grown because of the extra features on the Web pages etc

From my console I get the following message :-

<TX> at+s.httpdfsupdate=192.168.0.12,/outfile.img

<RX>  Invalid HTTPD_FS image, length (633215)

I am not sure if my image file is somehow corrupt or just too large.

My previous image files have worked perfectly from a PC set up as web server

and are approx 300k in length.

I have tried running Httpd_gen.exe a few times but the same results. 

Is there a maximum size permitted ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Gerardo GALLUCCI
ST Employee
Posted on September 02, 2016 at 17:58

Hi Paul,

1Mb flash memory is splitted in 2 different parts: half dedicated to FW-OTA, and half dedicated to FS-OTA. So, 500Kb is maximum allowed size for both commands.

Ciao

jerry