2018-07-13 11:12 PM
Hello everyone! I'm new here and this is my firt question.
I've been trying for a while to use the X-NUCLEO-IDW01M1, with poor success: I can't even build the example projects in the X-CUBE-WIFI1 software expansion package into System Workbench! But this is not what I'm asking about right now.
Few days ago I found this Wi-Fi training Hands-On (
) and finally I can see something runs. Unfortunately, I still encounter some issues:I hope you can help me as soon as possible.
I'm using the IDW01M1 with an STM32F401RE because of a university project, I can't change or upgrade these devices, and I have to use the Wi-Fi functionalities I'm trying to understand in a bigger and more complex project.
2018-07-16 01:35 AM
Dear,
following my comments:
1) please check the http service is enabled on SPWF01:
AT+S.GCFG=ip_use_httpd
# ip_use_httpd = 1
2) what do you mean with 'it redirects'? for a fast MiniAP setup you can keep pressed the SW2 button while resetting the IDW01M1, then connect your station to the MiniAP (ssid is something like iwm-XY-WZ-JK) and get captiveportal.net: you should get the firstset page.
3) please be sure the escape sequence is typed in one shot (<250ms).
Finally, can you share the FW version of your SPWF01 (AT+S.STS=version)?
For your information, a new FW (3.6.0) for SPWF01Sx has been recently released and available at
.2018-07-16 09:27 AM
Hello Elio,
thanks a lot for replying!
1) I checked the http service, it was disabled, now I enabled it
2) I mean 'captiveportal.net' redirected to 'www.tonymorella.com', but I'm gonna give another try following your instructions.
The FW version is 160129-c5bf5ce-SPWF01S.