2021-03-05 02:39 AM
2021-03-05 02:50 AM
Hi @ASpar.1 ,
you may find useful this application note.
It describes an application involving wireless Bluetooth Low Energy (BLE) communication between wearable nodes based on the BlueNRG-1 or BlueNRG-2 systems on chip.
-Eleon
2021-03-05 08:20 AM
thank you. I had already seen this document. The problem is that the power to which these devices transmit is not indicated, therefore with the measured RSSI value, I cannot get an idea of how far and intensely these devices are able to transmit. If they were set to -65 dbm and I measured -69, at a distance of two meters, as reported, it would be excellent, but if instead 0 dbm was set as Tx power, it would not be so great.
I need for an indoor localization system so i should have an idea about this.
2021-03-12 02:31 AM
Hi @ASpar.1 ,
you may find more info on the tx rx power oand other device characteristics on the chip datasheets, e.g. the BlueNRG-2 one.
I found also an interesting paper here on this application.
As side note, for the indoor navigation you could also consider the use of a pressure sensor (such as the LPS22HH) that can give you an accurate estimation on the height inside a building.
-Eleon