2019-01-12 7:12 PM
How to transfer audio files from the phone to a (BLUENRG+STM32+SDcard), without using additional software on the phone? I'm not sure, but I need an FTP profile. I need to realize the transfer of a sound file using the built-in Android / IOS functions on the device and play this track at the touch of a button on the device. Like single-mode BLE devices do not support FTP. Tell me where I am wrong and advise a solution that can solve my problem. Thank.
PS Maybe I'm wrong that I need FTP.
2019-01-12 8:31 PM
Or i need only OBEX OPP profile to send file from phone to device?
2019-01-18 11:48 PM
Help me please((((((((((