2017-03-15 2:48 AM
Hi,
What is the best way to generate custom BLE 128 bit UUIDs ?
How has ST generated the custom UUIDs in the firmware examples of Sensortile kit related to BLE ? For example, following are some UUIDs(in bold) in one of the firmware example :
/* Hardware Characteristics Service */
&sharpdefine COPY_HW_SENS_W2ST_SERVICE_UUID(uuid_struct) COPY_UUID_128(uuid_struct,0x00,0x00,0x00,0x00,0x00,0x01,0x11,0xe1,0x9a,0xb4,0x00,0x02,0xa5,0xd5,0xc5,0x1b)&sharpdefine COPY_ENVIRONMENTAL_W2ST_CHAR_UUID(uuid_struct) COPY_UUID_128(uuid_struct,0x00,0x00,0x00,0x00,0x00,0x01,0x11,0xe1,0xac,0x36,0x00,0x02,0xa5,0xd5,0xc5,0x1b)Is there a tool available for the same ?
Best Regards.
#ble-128-bit-custom-uuid #uuid #bluenrg #st-bluenrg2017-10-17 5:31 AM
Hi I am also having similar type of problem. For bluetooth module I want to add new characteristic under an existing service. But I am not sure how the UUID pattern is used. If you have resolved the issue then please share
#
#bluenrg
#st%20bluenrg
2017-10-18 6:25 AM
You are free to use any 128-bit UUID that you want, provided that it is not in the range of pre-allocated UUIDs, as specified below.
According to the Bluetooth specification:
'A UUID is a universally unique identifier that is guaranteed to be unique across
all space and all time. UUIDs can be independently created in a distributed
fashion. No central registry of assigned UUIDs is required. A UUID is a 128-bit
value.
To reduce the burden of storing and transferring 128-bit UUID values, a range
of UUID values has been pre-allocated for assignment to often-used, registered
purposes. The first UUID in this pre-allocated range is known as the
Bluetooth Base UUID and has the value 00000000-0000-1000-8000-
00805F9B34FB, from the Bluetooth Assigned Numbers
document. UUID values
in the pre-allocated range have aliases that are represented as 16-bit or
32-bit values. These aliases are often called 16-bit and 32-bit UUIDs, but it is
important to note that each actually represents a 128-bit UUID value.
The full 128-bit value of a 16-bit or 32-bit UUID may be computed by a simple
arithmetic operation.
128_bit_value = 16_bit_value * 2^
96
+ Bluetooth_Base_UUID
128_bit_value = 32_bit_value * 2^
96
+ Bluetooth_Base_UUID
'.Also, please notice that you can't use 16-bit or 32-bit values for user-defined services and characteristics, as they are reserved for registered purposes.
Best regards,
Antonio