cancel
Showing results for 
Search instead for 
Did you mean: 

Data rate value and TX information from BlueNRG1 Mesh?

FChou
Associate II

hi,

i am searching for the information about the data rate and TX power value in Mesh code where can i find this information ?

In datasheet the air data rate is about 1 Mbit/s is this data rate the same like for the BlueNRG-1 Mesh ?

Thank you

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
alok
Senior

Did you review the function  Appli_BleSetTxPowerCb for setting the Tx Power ?

The BLE-Mesh is for low data rate applications. You can consider 8bytes application data being transferred per 20ms of advertisement interval. Then the size of Mesh will define the total application throughput