2016-06-27 04:52 AM
Hello!
Is there a way to connect to an existing AP without hardcoding the SSID, login credentials etc? For example, using WPS. In the AT command spec there is a Table defining some errors where number 21 has the message ''Cannot use GPIO7. Reserved for WPSfeature'' but the meaning is set to ''!!!!Ignore!!!!''. Is this an upcoming feature? Or is there any other way to be able to connect to an arbitrary local AP?Regards,Pontus
2016-07-04 02:21 AM
WPS is not part of SPWF01Sx features. You can use miniAP firstset webpage, and fill target AP credentials