2019-07-23 3:54 AM
I am using STEVAL-BFA001V1B evaluation kit where I am trying to initialize the MCU on sensor board present in the kit.
I have connected ST-LINK/V2-1 programmer/debugger to the sensor board via an adapter board present in the same kit. The ST-LINK/V2-1 has a USB port which I connected to PC to dump the .bin file.
However an error saying 'the interface firmware failed to initialize/reset the target MCU' appears.
I saw a post in this forum saying this could be due to fault in power management system of sensor board which is working fine.
Your reply is deeply appreciated
Thanks in advance
-Chandrasekhar DVS