2015-10-11 6:14 AM
Hi everybody,
I have troubles to connect the SPWF01 with an AP using WPA2 privacy mode. When I try to connect, after Wind 25: association successful, I receive Wind 40: deauthentication:1 +WIND:19:WiFi Join:00:04:ED:61:FB:18 +WIND:25:WiFi Association with 'Alison' successful +WIND:40:WiFi Deauthentication:1 +WIND:74:Rejected found Network I have another AP and I can link with it using the same security mode and the same password, hence my code should be right. +WIND:19:WiFi Join:14:CC:20:9C:D5:4D +WIND:25:WiFi Association with 'Alison_EXT' successful +WIND:51:WPA Handshake Complete +WIND:24:WiFi Up:192.168.1.110 I did a scan and the APs are in WPA2 for sure: 1: BSS 00:04:ED:61:FB:18 CHAN: 06 RSSI: -59 SSID: 'Alison' CAPS: 0411 WPA2 2: BSS 14:CC:20:9C:D5:4D CHAN: 06 RSSI: -79 SSID: 'Alison_EXT' CAPS: 0431 WPA WPA2 WPS I think it could be a security issue because I can connect to the bad AP in Open mode. I searched the web for deauthentication:1. It is ''Unspecified failure'', so I can't have any clue from it. The module has the last FW version: 150410-c2e37a3-SPWF01S. Could you give me any hint? Thank you, Paolo2015-10-14 12:46 AM
Ciao Salvatore,
I'm sorry for the late reply. A PC Win8.1 and a smartphone Android work fine with Michelangelo Wave. I tried WEP 64 bits, password ''pippo'', and WEP 128 bits, password ''0123456789012''. In both cases also the SPWF01SA connects with the AP and I can ping it from the PC. The strangeness is when I try to connect the SPWF01SA using a wrong password: I cannot reach it anymore (right) but it says Wifi Up (wrong). Paolo2015-10-14 11:08 AM
Ciao Paolo,
I did the same test using our APs in WEP mode (both OPEN SYSTEM and SHARED KEY) but I cannot see the issue.If the password set in the module doesn't match the AP one, the module replies properly with:+WIND:19:WiFi Join:80:B6:86:6F:CF:72+WIND:45:Dot11 AuthIllegal 1/4+WIND:75:Rejected Association (0xF) I will continue the test with all our APs and I will give you a feedback.Did you observe the issue also using a different AP?ThanksCiaoSalvatore