cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot connect with AP

paolo23
Associate II
Posted on October 11, 2015 at 15:14

Hi everybody,

I have troubles to connect the SPWF01 with an AP using WPA2 privacy mode.

When I try to connect, after Wind 25: association successful, I receive Wind 40: deauthentication:1

+WIND:19:WiFi Join:00:04:ED:61:FB:18

+WIND:25:WiFi Association with 'Alison' successful

+WIND:40:WiFi Deauthentication:1

+WIND:74:Rejected found Network

I have another AP and I can link with it using the same security mode and the same password, hence my code should be right.

+WIND:19:WiFi Join:14:CC:20:9C:D5:4D

+WIND:25:WiFi Association with 'Alison_EXT' successful

+WIND:51:WPA Handshake Complete

+WIND:24:WiFi Up:192.168.1.110

I did a scan and the APs are in WPA2 for sure:

1: BSS 00:04:ED:61:FB:18 CHAN: 06 RSSI: -59 SSID: 'Alison' CAPS: 0411 WPA2

2: BSS 14:CC:20:9C:D5:4D CHAN: 06 RSSI: -79 SSID: 'Alison_EXT' CAPS: 0431 WPA WPA2 WPS

I think it could be a security issue because I can connect to the bad AP in Open mode.

I searched the web for deauthentication:1. It is ''Unspecified failure'', so I can't have any clue from it.

The module has the last FW version: 150410-c2e37a3-SPWF01S.

Could you give me any hint?

Thank you,

Paolo

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
Gerardo GALLUCCI
ST Employee
Posted on October 11, 2015 at 15:30

Ciao Paolo,

can you please share AP model, and FW version too?

ciao

jerry

paolo23
Associate II
Posted on October 12, 2015 at 10:43

Ciao Jerry,

AP model: Digicom Michelangelo Wave

FW version: 2.7.0.23(RUE0.C2)3.5.10.1

Paolo

Gerardo GALLUCCI
ST Employee
Posted on October 12, 2015 at 10:54

Can I ask you to update router FW to the lastest one?

Versioni RUE: 2.11.62.2RE0 - Versioni ZUE: 2.9.5.3ZUE

Thanks

j

paolo23
Associate II
Posted on October 12, 2015 at 12:38

I'm sorry, I don't do it...

my AP works well and I don't want to break its equilibrium.

It hasn't given me a problem in years of work.

Paolo

Nickname3786_O
Associate II
Posted on October 12, 2015 at 21:37

Ciao Paolo,

do you see the issue using all of the following settings (WPA mode/Cipher Suite)?

- WPA/TKIP

- WPA/AES

- WPA2/TKIP

- WPA2/AES

Thanks

Ciao

Salvatore

paolo23
Associate II
Posted on October 13, 2015 at 10:28

Ciao Salvatore, Gerardo,

I upgraded the AP FW and the problem is desapeared!

I have another oddity for you. Trying to connect to the AP in all the privacy modes I noticed that using WEP the SPWF01 gives me Wifi Up even though the password was wrong. Module however was not reacheble. This still happens after the AP FW upgrade.

Paolo

Gerardo GALLUCCI
ST Employee
Posted on October 13, 2015 at 10:34

Ciao Paolo,

in attach an howto use WEP. It's not so easy like WPA

Let us know if problem is still there.

Thanks

jerry

________________

Attachments :

WEP_key_config.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1Em&d=%2Fa%2F0X0000000bn5%2FiVT6evhEiXIPE64aqAwag28X35.VJZYdvGt5SBZHQiE&asPdf=false
paolo23
Associate II
Posted on October 13, 2015 at 10:43

Hi Gerardo,

I'm not saying that WEP doesn't work.

I was able to

use it

.

I'm saying that the module says connected even if it isn't.

Paolo

Nickname3786_O
Associate II
Posted on October 13, 2015 at 22:12

Hi Paolo,

could you please confirm that another device (PC, smartphone) works fine with the AP in WEP mode?

I found some threads on public forums where users claim issues after connecting a PC to Michelangelo Wave (in WEP mode).

Could you please also share with us the details of the WEP config used (WEP authentication, WEP encryption, Key 1 configured)?

Thanks

Ciao

Salvatore