2022-03-12 09:04 AM
buff_tx Error: Multiple errors reported.\ Failed to execute MI command: -var-create - * buff_tx Error message from debugger back end: -var-create: unable to create variable object\ Failed to execute MI command: -var-create - * buff_tx Error message from
2022-03-12 09:11 AM
Perhaps you can show or attach your code. The output from the build process, debugging, etc.
Indicate what STM32 part/board you're actually using.
2022-03-13 08:47 AM
Yes i can send the project
Can you send an address to send to
2022-03-13 08:56 AM