BNRG2A1 Terminates connection before reading service characteristics
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-10-17 10:10 AM
I am using the STM32 NUCLEOL476 with a X-Nucleo-BNRG2A1. I opened the example project for Central Device. The board scans and finds the BLE device. I can select the device and it will connect to it. Then it reads the Service then terminates. I have tried several different working BLE devices and the same problem occurs. This is the printout I get
------------------- START_CONNECTION -------------------
aci_gap_create_connection() OK
Device 0 connected
- address 00:a0:50:d2:22:99
- connection handle 0x0801
CONNECTION_COMPLETE
SERVICE_DISCOVERY
connection handle 0x0801
aci_gatt_disc_all_primary_services() OK
hci_disconnection_complete_event() unexpected reason: 0x08
CONNECTION_TERMINATED
GATT Procedure completed with error 0x41 (0x0801)
---------------- DISCONNECTION_COMPLETE ----------------
There is not much online regarding this except possibly supervision time needs to be increased. I havent found where in the example code to do this or if there is another issue causing it.
I am using rev3.3 X-Cube-BLE2, the the STMCubeIDE project.
Any help would be appreciated.
- Labels:
-
BLE
-
STM32L4 Series