2024-07-13 10:37 AM
I currently have a BLUENRG-M2SP connected via SWD to my STLink-V3PWR.
The issue is while my flasher can connect to the device it then cannot read the bootloader sector or flash the address memory.
Here is the log:
16:34:35.247: Waiting device to read bootloader (device connected by ST-Link) ->Device Connected
16:34:35.437: Device Identification -> BlueNRG-2
16:34:35.620: Read Bootloader Sector -> FAILED
16:34:36.038: Device Disconnection -> SUCCESS
My set up is:
In addition to this, I also have the boot pin connected to another PSU that would supply it with 3V6. I heard/read via the datasheet that at times it is neccessary to force the boot pin high. This forces the chip to go into the bootloader and ensuring that the SWD debug pins are open for connection.
So I have three questions.
Cheers for the feedback.
Solved! Go to Solution.
2024-07-14 02:19 AM
FYI
I have solved the problem. Here is the fix just in case it helps anyone in the future.
I have attached my setup below incase it helps.
2024-07-14 02:19 AM
FYI
I have solved the problem. Here is the fix just in case it helps anyone in the future.
I have attached my setup below incase it helps.