2021-03-19 5:50 AM
My evalboard seems to work. (I can flash the demo projects)
But when I try to use the GUI, it does not detect the device. "No Firmware detected on motherboard..."
It is successful to flash the Firmware STEVAL-IDB011V1/USB_CMSISDAP.hex but afterwards everything starts from the beginning.
What can I do?
Solved! Go to Solution.
2021-03-25 5:22 AM
Solved:
Did a clean step by step flash again. Now it works as expected:
Hold Reset, Plug USB, Maintenance Mode -> USB_CMSISDAP.hex
Drag&Drop -> DTM_UART_WITH_UPDATER.hex
BlueNRG GUI Update -> DTM_UART_FOR_UPDATER.bin
Had to remove JP5 for the first / second step. Do not remember.
Got an error before: error: The interface firmware FAILED to reset/halt the target MCU type: target
2021-03-25 5:22 AM
Solved:
Did a clean step by step flash again. Now it works as expected:
Hold Reset, Plug USB, Maintenance Mode -> USB_CMSISDAP.hex
Drag&Drop -> DTM_UART_WITH_UPDATER.hex
BlueNRG GUI Update -> DTM_UART_FOR_UPDATER.bin
Had to remove JP5 for the first / second step. Do not remember.
Got an error before: error: The interface firmware FAILED to reset/halt the target MCU type: target