cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG ACI protocol

ELema
Associate

Is there a document describing the bluenrg ACI protocol ? I intend to connect a windows computer to a X-NUCLEO-BNRG2A1 via UART, and use the default DTM firmware to do some basic evaluations.

I can see these possibilities:

  1. reverse-engineer BlueNRG-1_2 DK 3.2.1\Library\STM32L\Middlewares\ST\STM32_BlueNRG1\SimpleBlueNRG1_HCI to find out how commands are sent
  2. reverse engineer BlueNRG-1_2 DK 3.2.1\Project\BLE_Examples\DTM\src\DTM_cmd_db.c to find out how commands are received
  3. port BlueNRG-1_2 DK 3.2.1\Library\STM32L\Middlewares\ST\STM32_BlueNRG1\SimpleBlueNRG1_HCI to windows

All these are time consuming, and would not be needed if there was a document describing the ACI protocol. I could not find it, but does it exist somewhere ?

Thanks !

Eric Lemanissier

0 REPLIES 0