2021-09-16 12:59 AM
Is there any manual for BlueNRG-2 where I can find the register describtion? the point is to use UART but without HAL driver. I mean document like other STM32 MCU have.
BR KWT
2021-09-16 06:44 AM
Hello @KTarc,
I am not a BlueNRG expert, but the BlueNRG-2 datasheet describes the registers and should help you.
You can find other documents in the "Documentation" section of the ST official website.
Chahinez.
2021-09-16 06:46 AM
Those documents do not provide needed data.
2021-10-01 07:27 AM
I also cant find more information on the bluenrg1/2 chips. To be specific I need to use BlueNRG2 as network controller with host in external SoC. However the provided DTM firmware is not what I need. The DTM expose only LE part of some commands and therefore is not suitable for all type of scenarios.
2021-12-23 06:17 AM
It has something to do with the LL_MODE *** how is the DTM build. More documentation is needed from the ST.