2020-05-05 11:52 PM
Title somewhat covers it,
I have a custom circuit based off the Blue Tile eval kit BCN002V1 board. I'm trying to flash it with the host board and the BLE_SensorDemo.hex but I'm not seeing the board pop up in the comm ports when I connect it like I would the tile. Unfortunately I don't have much more info than that.
I guess my question would be is there something preloaded that allows the communication with the blue tile? Or can one communicate from a newly assembled board?
Thanks in advance!
2020-05-10 07:42 PM
Not quite sure about the question,
but i think you shall be able to get the answer from BLE_SensorDemo project in STSW-BLUETILE-DK :
2020-05-21 03:01 PM
This is still an ongoing issue, albeit slightly evolved from this original one. It was the microusb cable not transmitting data!