cancel
Showing results for 
Search instead for 
Did you mean: 

AT COMMAND MODE sp1ml hyperterminal

TARHAN SAMAH
Senior
Posted on November 15, 2017 at 15:54

ok now i got the firmware and download the binary to the sp1ml using st-link , looks it is downloaded , now i want to test the AT COMMAND mode using the hyperterminal , first let me tell you the hardware connections pins :

-SHDN  connected to 3,3v , always power up 

-mode0 to 0, it is command mode

-vdd 3,3v 

-gnd to gnd 

-rx of spirit to tx of hyperterminal 

-tx of spirit to rx of hyperterminal 

-reset to button 3,3v to 0volts

i use baudrate 9600 and CR after sending :

,  i opened hyperterminal after reset i got '?',   so i entererd to command mode '+++' no answer , i tried AT nthg comes from spirit,??? is there something i missed 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Mike Kay
Associate
Posted on January 29, 2018 at 20:08

I think the default Baud rate is 115200. Once you enter command mode, you can change the Baudrate.