cancel
Showing results for 
Search instead for 
Did you mean: 

STM8S103: UART1 Receiving String With Delay () and Multiple GPIO handle Problem

Jaydip Patel
Associate
 
/* Includes ------------------------------------------------------------------*/
 
#include "stm8s.h"
 
#include "stdio.h"
 
 
 
/**
 
 * @addtogroup UART1_HyperTerminal_Interrupt
 
 * @{
 
 */
 
/* Private typedef -----------------------------------------------------------*/
 
/* Private define ------------------------------------------------------------*/
 
 
 
#define Relay_1_Port (GPIOB)
 
#define Relay_1_Pin (GPIO_PIN_5)
 
#define Relay_1 '1'
 
 
 
#define LED_1_OFF_Port (GPIOC)
 
#define LED_1_OFF_Pin (GPIO_PIN_7)
 
 
 
 
 
#define Read_fun '0'
 
#define Write_fun '1'
 
 
 
#define HIGH '1'
 
#define LOW '0'
 
 
 
 
 
#define DEBUG_SERIAL_ECHO_BACK // fOR DEBUGGING
 
#define DEBUG_RECEIVED_FUNCTION_FROM_SERIAL
 
 
 
/* Private macro -------------------------------------------------------------*/
 
/* Private variables ---------------------------------------------------------*/
 
/* Private function prototypes -----------------------------------------------*/
 
 
 
static void CLK_Config(void);
 
static void UART1_Config(void); 
 
void Delay(uint32_t nCount);
 
char Serial_read_char(void);
 
void Serial_print_char (char value);
 
bool Serial_available();
 
void Serial_print_string (char string[]);
 
 
 
/* Private functions ---------------------------------------------------------*/
 
 
 
/**
 
 * @brief Main program.
 
 * @param None
 
 * @retval None
 
 */
 
static char *cmd = "ASDF-TC:" ;
 
static uint8_t cmd_cmpr = 0; 
 
void main(void)
 
{
 
 /* Clock configuration -----------------------------------------*/
 
 CLK_Config();  
 
 
 
GPIO_Init(Relay_1_Port, (GPIO_Pin_TypeDef)Relay_1_Pin, GPIO_MODE_OUT_PP_LOW_FAST);
 
Delay(100000);
 
GPIO_Init(LED_1_OFF_Port, (GPIO_Pin_TypeDef)LED_1_OFF_Pin, GPIO_MODE_OUT_PP_LOW_FAST);
 
Delay(100000);
 
 
 
 /* UART1 configuration -----------------------------------------*/
 
 
 
UART1_Config();
 
Delay(100000);
 
 while (1)
 
 {
 
  if (Serial_available()>0)
 
  {
 
   cmd_cmpr=0; // RESET 
 
   char data[20]={0};
 
   for (int i = 0; i < 8; i++)
 
   {
 
    data[i] = Serial_read_char();
 
     
 
    #ifdef DEBUG_SERIAL_ECHO_BACK
 
    Serial_print_char(data[i]);
 
    #endif
 
     
 
    if (data[i]==*(cmd+i))
 
    {
 
     cmd_cmpr=1;
 
    }
 
    else
 
    {
 
     cmd_cmpr=0;
 
     break;
 
    }
 
     
 
   }
 
    
 
   char Read_write_fun = Serial_read_char();
 
   char Relay_num    = Serial_read_char();
 
   char Write_High_Low = Serial_read_char();
 
    
 
   #ifdef DEBUG_RECEIVED_FUNCTION_FROM_SERIAL
 
   Serial_print_string("\n----- Received Command code --------\n");
 
   Serial_print_char(Read_write_fun);
 
   Serial_print_char(Relay_num);
 
   Serial_print_char(Write_High_Low);  
 
   #endif
 
    
 
    
 
    
 
   if (cmd_cmpr)
 
   {
 
     
 
     
 
    if (Read_write_fun == Write_fun)
 
    {
 
     if (Relay_num==Relay_1)
 
     {
 
      if (Write_High_Low == HIGH)
 
       GPIO_WriteHigh(Relay_1_Port, (GPIO_Pin_TypeDef)Relay_1_Pin);
 
       GPIO_WriteLow(LED_1_OFF_Port, (GPIO_Pin_TypeDef)LED_1_OFF_Pin);  // this is not working
 
       
 
      if (Write_High_Low == LOW)
 
       GPIO_WriteLow(Relay_1_Port, (GPIO_Pin_TypeDef)Relay_1_Pin);
 
       GPIO_WriteHigh(LED_1_OFF_Port, (GPIO_Pin_TypeDef)LED_1_OFF_Pin); // this is working
 
       
 
     }
 
      
 
    }
 
     
 
     
 
   }
 
   
 
    
 
    
 
      
 
    
 
  }
 
 
 
   // Delay(100000);  // If put this Delay then UART  not working properly 
 
   
 
 }
 
}
 
 
 
 
 
 
 
 
 
 void Serial_print_string (char string[])
 
 {
 
     while (UART1_GetFlagStatus(UART1_FLAG_TXE) == RESET); //wait for sending
 
  char i=0;
 
 
 
  while (string[i] != 0x00)
 
  {
 
  UART1_SendData8(string[i]);
 
  while (UART1_GetFlagStatus(UART1_FLAG_TXE) == RESET);
 
  i++;
 
 }
 
 }
 
 
 
 
 
 
 
 
 
char Serial_read_char(void)
 
 { 
 
  
 
  int read_count_var=0;
 
  while (UART1_GetFlagStatus(UART1_FLAG_RXNE) == 0)
 
  { 
 
   read_count_var++;
 
   Delay(1);
 
   if (read_count_var>=100) {break;}
 
 
 
   
 
  }
 
  while (UART1_GetFlagStatus(UART1_FLAG_TXE) == RESET);
 
  UART1_ClearFlag(UART1_FLAG_RXNE);
 
     
 
  return (UART1_ReceiveData8());
 
 
 
 }
 
 
 
 void Serial_print_char (char value)
 
 {
 
  UART1_SendData8(value);
 
  while (UART1_GetFlagStatus(UART1_FLAG_TXE) == RESET); //wait for sending
 
 }
 
 
 
 
 
 bool Serial_available()
 
 {
 
  if(UART1_GetFlagStatus(UART1_FLAG_RXNE) == 1)
 
  return TRUE;
 
  else
 
  return FALSE;
 
 }
 
 
 
 
 
 
 
/**
 
 * @brief Configure system clock to run at 16Mhz
 
 * @param None
 
 * @retval None
 
 */
 
static void CLK_Config(void)
 
{
 
  /* Initialization of the clock */
 
  /* Clock divider to HSI/1 */
 
  CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);
 
}
 
 
 
/**
 
 * @brief Configure LEDs available on the evaluation board
 
 * @param None
 
 * @retval None
 
 */
 
 
 
 
 
/**
 
 * @brief Configure UART1 for the communication with HyperTerminal
 
 * @param None
 
 * @retval None
 
 */
 
static void UART1_Config(void)
 
{
 
 /* EVAL COM (UART) configuration -----------------------------------------*/
 
 /* USART configured as follow:
 
    - BaudRate = 115200 baud  
 
    - Word Length = 8 Bits
 
    - One Stop Bit
 
    - Odd parity
 
    - Receive and transmit enabled
 
    - UART Clock disabled
 
 */
 
 UART1_Init((uint32_t)115200, UART1_WORDLENGTH_8D,UART1_STOPBITS_1, UART1_PARITY_NO,
 
          UART1_SYNCMODE_CLOCK_DISABLE, UART1_MODE_TXRX_ENABLE);
 
 
 
 /* Enable the UART Receive interrupt: this interrupt is generated when the UART
 
  receive data register is not empty */
 
 //UART1_ITConfig(UART1_IT_RXNE_OR, ENABLE);
 
  
 
 /* Enable the UART Transmit complete interrupt: this interrupt is generated 
 
   when the UART transmit Shift Register is empty */
 
 //UART1_ITConfig(UART1_IT_TXE, ENABLE);
 
 
 
 /* Enable UART */
 
 UART1_Cmd(ENABLE);
 
  
 
  /* Enable general interrupts */
 
// enableInterrupts();
 
}
 
 
 
/**
 
 * @brief Delay.
 
 * @param nCount
 
 * @retval None
 
 */
 
void Delay(uint32_t nCount)
 
{
 
 /* Decrement nCount value */
 
 while (nCount != 0)
 
 {
 
  nCount--;
 
 }
 
}
 
 
 
#ifdef USE_FULL_ASSERT
 
 
 
/**
 
 * @brief Reports the name of the source file and the source line number
 
 *  where the assert_param error has occurred.
 
 * @param file: pointer to the source file name
 
 * @param line: assert_param error line source number
 
 * @retval None
 
 */
 
void assert_failed(uint8_t* file, uint32_t line)
 
{ 
 
 /* User can add his own implementation to report the file name and line number,
 
   ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 
 
 
 /* Infinite loop */
 
 while (1)
 
 {
 
 }
 
}
 
#endif
 
 
 
/**
 
 * @}
 
 */
 
 
 
=================================================================
 
Command ASDF-TC:111 and ASDF-TC:110
 
 
 
 
 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0