2019-05-24 8:11 AM
Hi all,
I'v modified the example of MultiSensorRanging in STM32CubeExpansion_53L1A1_V2.1.0.
I'v fitted JMP U11 and U18, and modified the file X-NUCLEO-53L1A1.h as indicated.
All sensors renging but only the centered generates interrups!
#ifndef VL53L1A1_GPIO1_SHARED
/**
* @brief select use of shared interrupt
*
* Must be set to 0 (or not defined) for one interrupt per sensor
* Must be set to non 0 for shared interrupt line
* see @sa VL53L1A1_GPIO1_C_OPTION
*/
# define VL53L1A1_GPIO1_SHARED 0
#endif
/* X-NUCLEO-53L1A1.h */
#ifndef VL53L1A1_GPIO1_C_OPTION
/**
* @def VL53L1A1_GPIO1_C_OPTION
* @brief select GPIO1 to exti mapping for center or shared interrupt
*
* Set option value or un-define it to match with board configuration
* @li not defined or 0 : U14=On and U17=off => GPIO1_C = PA4
* @li defined and not 0 : U14=Off and U17=on => GPIO1_C = PC1
*/
# define VL53L1A1_GPIO1_C_OPTION 0
#endif
#ifndef VL53L1A1_GPIO1_L_OPTION
/**
* @def VL53L1A1_GPIO1_L_OPTION
* @brief control left sensor GPIO1 routing solder option
* @warning not used on shared interrupt config
*
* Set option value or un-define it to match with board configuration
* @li not defined or 0 : U10=on and U11=Off => GPIO1_L = PC7
* @li defined and not 0 : U10=off and U11=on => GPIO1_L = PA9
*/
# define VL53L1A1_GPIO1_L_OPTION 1
#endif
#ifndef VL53L1A1_GPIO1_R_OPTION
/**
* @def VL53L1A1_GPIO1_R_OPTION
* @brief control right sensor GPIO1 routing solder option
* @warning not used on shared interrupt config
*
* Set option value or un-define it to match with board configuration
* @li not defined or 0 : U18=on and U15=Off => GPIO1_R = PA10
* @li defined and not 0 : U18=off and U15=on => GPIO1_R = PB5
*/
# define VL53L1A1_GPIO1_R_OPTION 0
#endif
/* END X-NUCLEO-53L1A1.h */
/* main.c */
for (ToFSensor=0;ToFSensor<3;ToFSensor++){ //Reset the 3 ToF sensors on the expansion board
status = XNUCLEO53L1A1_ResetId(ToFSensor, 0);
}
for (ToFSensor=0;ToFSensor<3;ToFSensor++){ // Bring the sensors out of the reset stage one by one and set the new I2C address
switch(ToFSensor){
case 0:
Dev=&devLeft;
break;
case 1:
Dev=&devCenter;
break;
case 2:
Dev=&devRight;
break;
}
status = XNUCLEO53L1A1_ResetId(ToFSensor, 1);
Dev->comms_speed_khz = 400;
Dev->I2cHandle = &hi2c1;
Dev->comms_type = 1;
Dev->I2cDevAddr=0x52; // default ToF sensor I2C address
VL53L1_RdWord(Dev, 0x010F, &wordData);
printf("VL53L1X: %02X\n\r", wordData);
newI2C = Dev->I2cDevAddr + (ToFSensor+1)*2;
status = VL53L1_SetDeviceAddress(Dev, newI2C);
Dev->I2cDevAddr=newI2C;
VL53L1_RdWord(Dev, 0x010F, &wordData);
printf("VL53L1X: %02X\n\r", wordData);
status = VL53L1_WaitDeviceBooted(Dev); // Device Initialization and setting
status = VL53L1_DataInit(Dev);
status = VL53L1_StaticInit(Dev);
status = VL53L1_SetDistanceMode(Dev, VL53L1_DISTANCEMODE_SHORT);
status = VL53L1_SetMeasurementTimingBudgetMicroSeconds(Dev, 300000);
status = VL53L1_SetInterMeasurementPeriodMilliSeconds(Dev, 1000);
DetectionConf.DetectionMode = VL53L1_DETECTION_DISTANCE_ONLY;
DetectionConf.IntrNoTarget = 0;
DetectionConf.Distance.CrossMode = VL53L1_THRESHOLD_IN_WINDOW; //!< Trigger interrupt if value > thresh_low AND value < thresh_high
DetectionConf.Distance.Low = 100; // in mm
DetectionConf.Distance.High = 1000; //in mm
//status = VL53L1_SetPresetMode(Dev, VL53L1_PRESETMODE_AUTONOMOUS);
status = VL53L1_SetThresholdConfig(Dev, &DetectionConf);
status = VL53L1_GetThresholdConfig(Dev, &DetectionConf);
status = VL53L1_StartMeasurement(Dev);
printf("Low: %d, High: %d, IntrNoTarget: %d, Mode: %d, CrossMode: %d\r\n", DetectionConf.Distance.Low, DetectionConf.Distance.High, DetectionConf.IntrNoTarget, DetectionConf.DetectionMode, DetectionConf.Distance.CrossMode );
}
2019-05-25 3:03 AM
I've found the bug!
The GPIO9/10 must be set as GPIO4 (center sensor): i.e. PULLUP and IT_RISING:grinning_face_with_sweat:
/*Configure GPIO pin : VL53L1X_INT_Pin */
GPIO_InitStruct.Pin = VL53L1X_INT_Pin_Center|VL53L1X_INT_Pin_Left|VL53L1X_INT_Pin_Right;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(VL53L1X_INT_GPIO_Port, &GPIO_InitStruct);
2019-06-04 7:53 AM
Well done. I didn't know that. =)