cancel
Showing results for 
Search instead for 
Did you mean: 

VL6180x TOF Sensor VCSEL Continuity Test Error

NPate.14
Associate

On our prototype circuit boards with VL6180x sensors there are 6 sensors per board. On a couple of our prototype boards (about 10% of our boards) we have seen just a single sensor able to respond over I2C but cannot start ranging. The result range status register always reports a  result__range_error_code: 1 - VCSEL Continuity Test error. I2C communications are fine and all other 5 sensors are able to range.

What is this power up test doing and what could cause this error?

1 REPLY 1
John E KVAM
ST Employee

It's a power issue.

The ToF chips from ST use 20mA when they are running. But that is an average during the 10ms or so it takes to get a range.

At the micro level the laser turns on and off at about a 30% duty cycle and during that 'on' the sensor draws quite a bit of power.

We believe this is your issue.

Bigger regulator perhaps?


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.