cancel
Showing results for 
Search instead for 
Did you mean: 

VL6180 Optimal Settings for Acuracy

gerbers
Associate

I am using the VL6180 (not the X version).  This is TOF only.  When reading in continuous mode, I'm getting a tolerance of +/- 1mm and sometimes more.  I'll list my settings below.    My application will measure distances from 10mm to 100mm.  Right now I have the inter-measurement period set to 500ms and this is flexible.  How can I optimize my settings further for accuracy? thanks

 

 

 

 

 

VL6180_WriteByte(0x0207, 0x01);  
VL6180_WriteByte(0x0208, 0x01);  
VL6180_WriteByte(0x0096, 0x00); 
VL6180_WriteByte(0x0097, 0xfd);  
VL6180_WriteByte(0x00e3, 0x00);  
VL6180_WriteByte(0x00e4, 0x04);  
VL6180_WriteByte(0x00e5, 0x02);  
VL6180_WriteByte(0x00e6, 0x01);  
VL6180_WriteByte(0x00e7, 0x03); 
VL6180_WriteByte(0x00f5, 0x02);  
VL6180_WriteByte(0x00d9, 0x05); 
VL6180_WriteByte(0x00db, 0xce);  
VL6180_WriteByte(0x00dc, 0x03);
VL6180_WriteByte(0x00dd, 0xf8);
VL6180_WriteByte(0x009f, 0x00);
VL6180_WriteByte(0x00a3, 0x3c);
VL6180_WriteByte(0x00b7, 0x00);
VL6180_WriteByte(0x00bb, 0x3c);
VL6180_WriteByte(0x00b2, 0x09);
VL6180_WriteByte(0x00ca, 0x09);
VL6180_WriteByte(0x0198, 0x01);
VL6180_WriteByte(0x01b0, 0x17);
VL6180_WriteByte(0x01ad, 0x00);
VL6180_WriteByte(0x00ff, 0x05);
VL6180_WriteByte(0x0100, 0x05);
VL6180_WriteByte(0x0199, 0x05);
VL6180_WriteByte(0x01a6, 0x1b);
VL6180_WriteByte(0x01ac, 0x3e);
VL6180_WriteByte(0x01a7, 0x1f);
VL6180_WriteByte(0x0030, 0x00);

 // Recommended : Public registers - See data sheet for more detail 
VL6180_WriteByte( 0x0011, 0x30); // Active high. Interrupt enabled
VL6180_WriteByte( 0x010a, 0x30); // Set the averaging sample period (compromise between lower noise and increased execution time)
VL6180_WriteByte( 0x003f, 0x46); // Sets the light and dark gain (upper nibble). Dark gain should not be changed.
VL6180_WriteByte( 0x0031, 0xFF); // sets the # of range measurements after which auto calibration of system is performed 
VL6180_WriteByte( 0x002e, 0x01); // perform a single temperature calibration of the ranging sensor 

// Optional: Public registers - See data sheet for more detail 
VL6180_WriteByte( 0x001b, 0x31); // Set default ranging inter-measurement period to 500ms (changing from 100ms or 0x09 to 500ms 0x31)
VL6180_WriteByte( 0x0014, 0x04); // Configures interrupt on New sample ready 

VL6180_WriteByte(SYSRANGE_MAX_CONVERGENCE_TIME, 0x3F);  // 0x14 = 20ms
VL6180_WriteByte(SYSRANGE__START, 0x03);  // Bit 1 = 0 (single shot).  Bit 1 = 1 (continuous mode).

 

 

 

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Zhiyuan.Han
ST Employee

Hi 

 

From your shred range result performance, I think +/-1mm is already the best case with 6180 sensor, if you want more accuracy, what I can suggest is applying a post-process rolling average if possible.  rolling average will give you a better accuracy but will lead time legacy, you can try with still or low speed target, not suggested for fast moving target.

 

Br

Zhiyuan.Han


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Zhiyuan.Han
ST Employee

Hi 

 

From your shred range result performance, I think +/-1mm is already the best case with 6180 sensor, if you want more accuracy, what I can suggest is applying a post-process rolling average if possible.  rolling average will give you a better accuracy but will lead time legacy, you can try with still or low speed target, not suggested for fast moving target.

 

Br

Zhiyuan.Han


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.