2024-04-30 07:51 PM
Hello,
We received an EOL status notification for our current sensor VL6180 and I found the VL53L4CD as a substitute for this TOF proximity sensor. We would like to know how long this device will be active, as the VL6180 is now on EOL.
Can you also connect us to one of your Field app engineers to discuss further the differences in application between the VL6180V1NR/1 and VL53L4CD? Thank You.
Regards,
Jerald
Solved! Go to Solution.
2024-05-02 07:41 AM
The ST Imaging group - that builds the ToF sensors guarantees 7 years of production on all our parts. The VL6180 lasted more than 10. And we would have kept it in production, except we can no longer procure some of the optical elements.
The VL53L4CD just came out. So, it has at least 6 more years to run. My guess is that it will run longer though. We will not have procurement issues we had on the 6180.
As to the FAE - I will send you an email and we can talk.
- john
2024-04-30 09:31 PM
The product page indicates a SEVEN year commitment, see small (7) icon.
Check the support pages for local sales offices.
2024-05-01 12:52 AM
VL6180 no eol
2024-05-01 01:12 AM - edited 2024-05-01 01:12 AM
VL6180 NRND
Available until January 2026, per page.
2024-05-01 02:19 AM
Based on Digikey the Last Time Buy Date is on 3/28/2025. After that, the status eventually changed to OBSOLETE.
That's why we are asking if the VL53L4CD can be used as an alternate part for the VL6180V1NR/1.
2024-05-02 07:41 AM
The ST Imaging group - that builds the ToF sensors guarantees 7 years of production on all our parts. The VL6180 lasted more than 10. And we would have kept it in production, except we can no longer procure some of the optical elements.
The VL53L4CD just came out. So, it has at least 6 more years to run. My guess is that it will run longer though. We will not have procurement issues we had on the 6180.
As to the FAE - I will send you an email and we can talk.
- john
2024-05-07 07:19 AM
The VL53L4CD is the recommended part to be used to replace the VL6180.
Documentation to help on the migration with an example code is coming soon.
2024-05-07 08:45 AM
Maybe I can fill in some details here.
Anne is right in that the VL53L4CD is the part you should look at. But it's not a direct replacement.
The part is just a bit smaller, has a different pin out, and uses different software.
So, you need a re-design.
But...
The VL53L4CD is a better sensor. Ranges people up to the full 1.3Meters.
The L4CD has a completely invisible 940nm VCSEL (laser light).
The L4CD has a narrower 18-degree Field of View. (Versus 27 degrees)
The L4CD is more accurate - and linear down to 0.
The L4CD has easier software.
The cost is in the same range as you were paying.
And the L4CD is pin and shape compatible to the VL53L4CX if you ever need more performance.
(If you go from the L4CD to the L4CX, swap the parts, change the API (almost the same function calls), and you can range to some 6M.)
If you were using the Ambient Light Sensor of the VL6180X, you will need a separate ALS chip. ST makes a tiny one - the VD8283. Consider that one.
And, of course, you can read the transition documentation when it comes out.
- john