cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L8CX SPI doesn't work properly

pshih
Associate II

Hi everyone: I am working on a project with VL53L8CX Time-of-Flight sensor from Pololu. I integrated it with NUCLEO-H755ZI-Q board over SPI interface based on the example and driver provided in the STMicro en.STSW-IMG040 software package. I configured the SPI3 (MCLK, MISO, and MOSI) on the CN7 to communicate with the sensor. I also have PA4 for SPI3_NSS and PC7 for /PLn signal. The project compiled successfully. However, I believe I am not able to read the registers properly.

 

The firmware reads the "device_id" and "revision_id" from the sensor in the vl53l8cx_is_alive() to determine if the sensor exists. The return values different every time I tried to read. I was able to capture the protocols on the scope, and confirmed the reading values are match with the data shown on the scope. The following scope capture shows the communication:

1. Sending 0x00 to address 0x7fff. The yellow signal is for the MCLK, blue for MOSI, purple for MISO, and green for /CS.

pshih_0-1725544500633.png

2. Receiving 0x0 from address 1 for "revision_id".

pshih_1-1725544500633.png

3. Another reading 0x4 from address 1 for "revision_id".

pshih_2-1725544500633.png

I tried to pull up the MISO signal to 3.3V by 10K resister or pull-down to GND with 47K resister. They don't resolve the issue. Tried different communication baud rate and they don't help. I also tried different module and they seems to have the same issue. At this point, I am not sure if the issue I am facing is in the hardware or software. I am looking forward to hearing your opinion and suggestions. Thanks!

11 REPLIES 11

Thank you for your reply. In that case, may I ask what frequency of ranging data you are able to get at 1000kHz with I2C? I'm hoping to be able to reach 60 Hz scanning frequency with my VL53L8CX.

pshih
Associate II

I don't think the ranging frequency is result from the communication speed. Based on my understanding, the maximum ranging capabilities for 4x4 in continuous mode is 30 Hz and 8x8 is 15Hz.