Skip to main content
MBabu.2
Associate II
Jun 22, 2021 7:35 AM UTC
Solved

Vl53l1x sensors from Pololu

Hey, For a project I am using multiple Vl53L1X sensors from ST and the driver I used is

https://github.com/rneurink/VL53L1X_ULD/tree/94b88bc06ef44950ec3a5fd50b2f0287c23c5ad7

It worked perfectly and am not having any issues.

But am planning to use multiple VL53L1X sensor from Pololu.

Can you tell me some of the difference between them (i.e.) Should I add external resistors for the Xshut pin and If I can use the same driver for both the sensors

Thank you so much

This topic has been closed for replies.
kwc
kwcBest answer
Associate II
Jul 16, 2021 3:21 AM UTC

Hi, Kevin from Pololu here. One thing to note is that, unlike on ST's VL53L1X-SATEL, the XSHUT and GPIO1 pins on our VL53L1X carrier are not level-shifted. That means you should avoid driving XSHUT high if you are using a 5V controller.

Since our board pulls XSHUT up to 2.8V by default, you can simply drive it low when you need to disable the sensor, then return the pin to a high-impedance state (set it to an input) to let the carrier board pull it up and re-enable the sensor. Alternatively, if you are using code that does drive the pin high and prefer not to change it, you can add a resistive voltage divider (or other level shifter) between the microcontroller and the XSHUT pin.

John, thanks for the kind words about our boards!

- Kevin

2 replies

John E KVAM
ST Employee
Jun 22, 2021 3:53 PM UTC

I love what the folks at Pololu have done with our sensor. Some people don't like the form-factor of the ST boards, so having a choice is fantastic.

(There are other companies that integrate our sensor - and I like them too.)

The 'trick' to using multiple sensors is that the all come up at the same address. And that clearly does not work.

So put them all in reset by dropping the XSHUT line.

Then bring one up, and issue the "change address" command.

Then bring the next one up and change it's address as well.

Repeat as often as you need.

I have a system with 9, although I've heard of a system with 12 sensors in it.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
kwc
kwcBest answer
Associate II
Jul 16, 2021 3:21 AM UTC

Hi, Kevin from Pololu here. One thing to note is that, unlike on ST's VL53L1X-SATEL, the XSHUT and GPIO1 pins on our VL53L1X carrier are not level-shifted. That means you should avoid driving XSHUT high if you are using a 5V controller.

Since our board pulls XSHUT up to 2.8V by default, you can simply drive it low when you need to disable the sensor, then return the pin to a high-impedance state (set it to an input) to let the carrier board pull it up and re-enable the sensor. Alternatively, if you are using code that does drive the pin high and prefer not to change it, you can add a resistive voltage divider (or other level shifter) between the microcontroller and the XSHUT pin.

John, thanks for the kind words about our boards!

- Kevin