2024-12-20 1:54 PM
#define RANGE_ERROR_DISTANCE_BELOW_DETECTION_THRESHOLD 0x03
#define RANGE_ERROR_OTHER 0xFF
Hi ST,
Some of our production devices are receiving the above errors.
Can someone help me with understanding what might cause these errors?
Thanks,
Will
Solved! Go to Solution.
2024-12-24 11:35 AM
The first one is easy - the sensor detected an object at some close distance and then applied the offset correction. Unfortunately, after the correction, the distance is below zero. And we were forbidden to return negative numbers, so we generated an error instead.
double check the offset correction. I fear it's too large in the negative direction.
The FF error is a bit more difficult. Something went wrong with the range and the sensor could not tell what. But the numbers the sensor was getting made no sense, and so it returned an "unspecified error".
One would have to know what was going on in order to figure it out. Massive motion might have caused it, but more likely it is two factors mixed. Something like massive motion in addition to close distances.
The FF doesn't show up very often unless something is going on with the target. Perhaps you have a small one in front of a large far one, and maybe some motion is causing the A range to not align with the B range.
(Under the covers, the A range and B range use different pulse repetition intervals to detect radar aliasing. But the ranges should align.)
- john
2024-12-24 11:35 AM
The first one is easy - the sensor detected an object at some close distance and then applied the offset correction. Unfortunately, after the correction, the distance is below zero. And we were forbidden to return negative numbers, so we generated an error instead.
double check the offset correction. I fear it's too large in the negative direction.
The FF error is a bit more difficult. Something went wrong with the range and the sensor could not tell what. But the numbers the sensor was getting made no sense, and so it returned an "unspecified error".
One would have to know what was going on in order to figure it out. Massive motion might have caused it, but more likely it is two factors mixed. Something like massive motion in addition to close distances.
The FF doesn't show up very often unless something is going on with the target. Perhaps you have a small one in front of a large far one, and maybe some motion is causing the A range to not align with the B range.
(Under the covers, the A range and B range use different pulse repetition intervals to detect radar aliasing. But the ranges should align.)
- john