cancel
Showing results for 
Search instead for 
Did you mean: 

"VL53L5CX_ULD_driver_1.3.1" and "CubeIDE_F401RE_Example" I could compile and run the project but when i try to debug it, I will always end up in the Hard Fault Handler. Has anyone an idea why this is happening?

dmeise
Associate II
 
1 REPLY 1
John E KVAM
ST Employee

I'm not sure but the firmware in the VL53L5 hates to be re-loaded. if it works and then you try to debug, you might be trying to re download the firmware, without powering down the sensor.

could that be it?

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.