cancel
Showing results for 
Search instead for 
Did you mean: 

Custom project requirement for ToF sensor

vishnusf
Associate II

HI,

I am using VL53L1 sensor for a custom project. I had some queries regarding the sensor,

1) what is the integration time for the SPAD sensor?

2) What is the max sampling rate of the SPAD sensor (ADC conversion)? What is the sampling frequency of the SPAD sensor?

3) I see that u mention the sensor having I2C speed of 400khz to 1MHZ, when operating at low speed does that mean the sensor is being sampled at lower rate.

4) I need to getSignal rate from each pixel, is that possible?. what is the maximum number of non overlapping pixel signal rate i can get ?

5) Could u please suggest an alternate sensor with appropriate MCU board that is compatible and easy to program and has many resources.

 

Thak you

0 REPLIES 0