cancel
Showing results for 
Search instead for 
Did you mean: 

Conecting B-CAMS-OMV with STM32MP257F-EV1

cbcosta
Associate

Hi, im planing on running computer vision DL models on multiple STM32 boards. At this moment I will compare a STM32MP256F-EV1 with a STM32H747-DISCO, however i only bought the B-CAMS-OMV and is not the same connector on the MP board. IS there any way o run this camera module on both board, can I just get an adapter from the 30-pin ZIF to the CSI connector?Also i dont is the any suplementary information about the ZIF connector

0 REPLIES 0