cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot conect to STEVAL-STWINBX1

aag
Associate II

Hello, 

I have received the STEVAL-STWINBX1 evaluation kit and am trying different demos to see how it works. 

At first I was programming the board with different examples (STM32CubeFunctionPack_STBOX1_V1.5.0) but I was having problems afterwards. Once the programming was done, I was trying to connect to the board via BLE Sensor App but my board didn't appear until I pressed RESET. Then, I read an issue on this community where a user was having a similar problem and the solution was to program the binary file on Bank 2 (Start address: 0x08100000). 

The problem still persists but now, once I connect the board to my computer, the computer doesn't detect it and the only LED blinking is LED_C. I don't know what to do, because I can't reset the board and I can't connect it to the computer either to program it again... 

Any suggestions?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
aag
Associate II

Forgot to say I'm trying to detect the board with the computer pressing USER button before connecting it to the computer, but still it doesn't work.