Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL6180X range measurement issue

Hello,I have following issue.For distance 0 mm - 60 mm the result of range measurement is always the same (0x20)step by step code:GPIO0 set High.Range measurement start: write 1 to reg 0x0018Wait 100msRead range status: read register 0x004DRead range...

MChla.1 by Associate
  • 1708 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L0X AVDD voltage

Hi everyone,I was wondering if it is possible to supply my VL53L0X with a 3V3 voltage?According to the datasheet, the 3V3 respects the recommanded operating condition.But when I look for example board from ST or other vendors, there is always a conve...

0690X000008iXO0QAM.jpg
Deadror by Associate
  • 4128 Views
  • 4 replies
  • 0 kudos

VL531L1 measurements always FF.

I have rewritten the C app for the VL531 in LAIRD SmartBasic in order to drive the VL531 from a BT module (BL652). I communicate OK with the VL531 over I2C but when I sent the start command (and after I get a Data Ready from register 0x31 as shown be...

TChar.288 by Associate II
  • 1956 Views
  • 2 replies
  • 0 kudos

Resolved! Can we measure the frequency of the beam (VL53L0X) ?

Hello Guys,I hope you all are doing well.I am working on a project that with the VL53L0X ToF Sensor and ESP modules.The sensor works great and i am trying to get deeper into its reads because what i need.I am trying to build a frequency meter using t...

SSilv by Associate
  • 3566 Views
  • 7 replies
  • 0 kudos

Could not receive the true unswer from VL53L1

Gentlemen! Sorry for bothering you.I try to use VL53L1 with the Light Driver. The power level is 3.0 V, so I changed the Initialization data array, cell 0x2E from 0x00 to 0x01 and cell 0x2F from 0x00 to 0x01. I wait for the Device ready (SensorState ...

niltec by Associate II
  • 2257 Views
  • 4 replies
  • 0 kudos

Problems calibrating VL53L0X ToF distance sensor (VL53L0X_perform_offset_calibration, VL53L0X_perform_xtalk_calibration). bug?

RoutineVL53L0X_perform_offset_calibration from src/core/src/vl53l0x_api_calibration.cpp is giving strange results. By my opinion the problem is in uint16_t sum_ranging which should be of type uint32_t due to later bit shifting (<<16), which needs to ...

GPodr.1 by Associate II
  • 2875 Views
  • 3 replies
  • 0 kudos