User Activity

Gentlemen! Sorry for bothering you.I try to use VL53L1 with the Light Driver. The power level is 3.0 V, so I changed the Initialization data array, cell 0x2E from 0x00 to 0x01 and cell 0x2F from 0x00 to 0x01. I wait for the Device ready (SensorState ...
Posted on November 03, 2016 at 11:22Gentlemen!I try to use chip ST95HF. I am a beginner in NFC. I need to develop Peer to Peer connection. What protocol should I use for it?I can not see of the emitted field at 13,56 MHz.I initialized of the chip to...