2019-05-24 3:52 AM
2019-05-24 10:01:31.578471543 | processPps()
2019-05-24 10:01:31.711095091 | $PSTMPPSDATA,1,1,1,0,0,0,0.500000,0,713,248,0,0,0,0,0,36,3,11,18,4,0,1.301e-08,65473955.16,25999998.74*16
2019-05-24 10:01:31.739373411 | $PSTMUTC,100135.000,24052019,1242727295,18,2*57
2019-05-24 10:01:31.739501850 | unixtime 1558692095 dUnixtime 0.000000013010 leapSec 18 leapSecValid 2
2019-05-24 10:01:32.578423766 | processPps()
Here previous PPS came at 10:01:31.578471543 local time
next at 2019-05-24 10:01:32.578423766
My understanding that quantization error from $PSTMPPSDATA 1.301e-08 should be added to next PPS signal to have precise time of the PPS. Am I right?
Following this logic $PSTMUTC should be the same next PPS second. Is this true?
Thank you in advance!
Ruslan
2019-05-31 5:04 AM
Hi
It seems you are using the Teseo-SDK.
The GNSS Community is targetting GNSS Binary Image solution.
Could you open a discussion with your relevant FAE?
Thanks
Regards
Francesco
2019-05-31 6:55 AM
Hi, Francesco!
I'm not using Teseo-SDK. I'm using UART to communicate with the module and digital signal 1PPS.
So I have incoming PPS number N
then group of NMEA messages by UART
then next PPS number N+1
as you can see in log in my first message with times attached.
Seconds switched on PPS coming. My question is
$PSTMUTC give number of a second starting from next PPS? Or this is the number of the current second started from previous to the $PSTMUTC message PPS signal?
This is a question about how binary image generates messages and PPS signals.
Best regards
Ruslan
2019-06-04 2:23 AM
Ciao
The UTC time information reported in the $PSTMUTC NMEA message are used to evaluates the Next PPS signal.
The $PSTMPPSDATA reports against which UTC time the PPS has been evaluated/generated.
Hope this helps
Regards
Francesco
2019-06-06 1:34 AM
Thank you, Francesco! This is useful information for me.
Can you also take a look at previous branch with attenuator tuning question (How to increase attenuation value in Teseo III RF front-end?)?
Values you suggested:
CDB-140 @ 0x0A
CDB-141 @ 40
if it helps, you can also tests different vales for CDB-141 (140 is mandatory @ 0x0A)
Does not work. What we can do to troubleshoot?
Best regards,
Ruslan