cancel
Showing results for 
Search instead for 
Did you mean: 

Teseo-LIV3F, no satellite position.

Sergei
Associate II

Hello, Can you help me?

I assembled a module on the Teseo-liv3f basis with a passive antenna (A25-4102920-AMT02). And I can not get the coordinates in nmea messages (screenshot in attach). What could be the problem?

Thank you.

This discussion is locked. Please start a new topic to ask your question.
24 REPLIES 24
Karim RAMSI
ST Employee

​7 44

Francesco Virlinzi
ST Employee

Ciao Francesco, Karim

The module in your hands isn't the final one.

It's a prototyping sample built in ~Nov 2017.

On board there isn't the final firmware.

We could plan a firmware-update of the module to promote the module to the final firmware.

@Francesco, On which board are you testing the module?

Thanks

Ciao

Francesco

Ciao Francesco and Karim,

The module is on a proprietary testing board. Here below the FW versions:

OS20LIB_4.3.0_ARM

GPSAPP_2.4.0.1_ARM

BINIMG_4.6.8.1_ARM

SWCFG_8204941a

WAASLIB_2.20.0_ARM

STAGPSLIB_5.1.0_ARM

STA8090_622bc043

GNSSLIB_8.4.10.16.3_ARM

Can I update the firmware by myself using the tool STA808x/9x Firmware Upgrade?

Where can I download the bin file?

Best regards

Francesco

Ciao Francesco

> Can I update the firmware by myself using the tool STA808x/9x Firmware Upgrade?

if in your board you can reset the module (just with a simple push-button or similar..) yes you can.

> Where can I download the bin file?

We will send the binary by email.

Is it ok?

Thanks

Ciao

Francesco

Ciao Francesco,

I can force the Reset pin to a low level (pin9 - SYS_RESETn) as described in the manual: "When the user wants to update the Teseo-LIV3F, Teseo-LIV3F must be powered and under reset; the user must configure the tool, select binary image and start firmware upgrade process. Only when the process has started, user must take Teseo-LIV3F out of reset."

Thank you, Francesco and Karim.

Francesco

Ciao Francesco

Perfect! You already have what you need ;)

You can go ahead with firmware-update.

Let us know.

Ciao

Francesco

After the upgrade, now it is working as I expected.

Great.

Thank you very much!

Francesco

Ciao Francesco

Perfect.

Let us know if the 4 hours issue is still there.

Thanks

Ciao

Francesco

Ciao Francesco,

I made several tests and Teseo, with the FW update, is working: it receives GPS and GLONASS.

I have one more question: how can I receive GALILEO satellite? Is there a configuration/enable?

Teseo-Suite require an activation key to unlock some feature, how can I have that?

Ciao

Francesco

Ciao Francesco

To enable Galileo you have to reconfigure the module.

Have a look into the attached presentation (slide 7) where all the possible configurations are listed (with related command).

For Teseo-Suite you can ask activation key to the Teseo-suite support.

Hope this help

Ciao

Francesco

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.