2019-09-05 2:16 AM
Hello,
I just integrated a Teseo Module on a custom design and was rewarded by a fix position at first power-on (luck of the beginner I guess) within 10 minutes.
I2C reading works well on startup and I can feed the steam to the teseo-suite where it is correctly interpreted. For that, I wrote an I2C to serial translator into the BNRG hosting the whole stuff (using AN5203 as guide).
Unfortunetly, as soon as I try to write to the module (via I2C), the first write completes (writing to register 0xFF) but the next read get me a repeated stream of same ascii char (random ones like '.', 'e', etc...and not an echo of the char I sent) and end-up with I2C clock tied low forever, locking down the I2C channel (transaction never ends).
As my design have a 'main power switch' on the teseo module, my program can detect that and power down then up the module and everything restart normally.
I have tried writing 1, 4 or many more bytes in one transaction. Nothing works but more than one byte at a time may lock-down the write transaction itself.
Is there any known issue ?
Thanks.
Remy.
Ps: module marked "904 GAS60", used at 400kHz.
2019-09-05 6:10 AM
FYI, I found my error:
When writing of reading from Teseo, do not use register adressing (as mentionned as '0xFF is FIFO read/write register' somewhere in UM2229).
Just read/write without any register address and all goes fine.
Thanks.
Remy.
2019-09-06 2:10 AM
Ok.
Perfect.
Eenjoy with Teseo-LIV3F
Ciao
Francesco