2021-07-24 3:59 AM
I want to use the teseo LIV3f GNSS module as an I2C positioning sensor and i am following the AN5203. However, when i send the configuration over I2C, the GNSS module responds to all the commands with corresponding OK message except for the $PSTMSAVEPAR command. It just echoes the command back without OK message. This command works only over UART. (I even tried sending the configurations over I2C and sending just the $PSTMSAVEPAR over UART, and this works). I would really like some help with this.
Thanks in Advance !