GNSS positioning

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Getting Time Based On The Place I Live

Hi everyone,I have designed a module with STA 8089GA which works properly. It gives me the exact position and fixes in less that a minute. I wanted to read time with this module. When I tried "PSTMGETRTCTIME" and "PSTMRTCTIME", it gives me time based...

Resolved! Issues on Setting Parameter

Hi, I have tons of question about the command $PSTMSETPAR and some related command:​First of all, I would like to change the NMEA Baudrate to 38400, as the software manual said, I should transfer​"$PSTMSETPAR,1102,0x8""$PSTMSAVEPAR"​and NMEA gives me...

0690X000006DBGRQA4.jpg
PTsen by Associate III
  • 2489 Views
  • 8 replies
  • 0 kudos

No GNSS message after cold start

Hi, after playing it for a while, I am able to communicate with the X-NULCEO-GNSS1A1 via USARTBut the altitude and longitude are not correct, it is not changing. Not knowing what to do, I decided to perform a cold start by sending the command "$PSTMC...

0690X000006D1HUQA0.jpg
PTsen by Associate III
  • 1066 Views
  • 6 replies
  • 0 kudos

Resolved! Can't communicate properly with X-NUCLEO-GNSS1A1

Hi, as the title said, I am having the hard time communicating with X-NUCLEO-GNSS1A1The GNSS module is communicate via USART (can't communicate via I2C, but this is the other problem)the code is written as follow:void usart_setup(void) { // so...

0690X000006CuzcQAC.jpg
PTsen by Associate III
  • 2567 Views
  • 6 replies
  • 0 kudos

Wake-Up Status of Teseo-LIV3F

Hi guys, i'm working with the GNSS expansion board X-NUCLEO-GNSS1A1, plugged to STM32F411RE Nucleo board. I looked inside the X-Cube GNSS1 expansion software package, which provides also some ready-to-be-built examples. I've chosen the simpler one, "...

How do i interpret 2D / 3D Acc. in Teseo-Suite Pro?

I have the Teseo-Liv3f eval kit and it finds 9 sats and i have 3D fix.  The lat/long/alt values are very stable but i cannot find any description of 2D and 3D Acc.  It seems the accuracy should be very "good" so what is the unit of these large number...

0690X000006CB8BQAW.png
TLubk by Associate II
  • 686 Views
  • 2 replies
  • 0 kudos