cancel
Showing results for 
Search instead for 
Did you mean: 

STA8100-EVB-T5DR question

iverson3ya
Associate

"I would like to ask a few questions:

  1. Initially, I was able to use the EVB-T5DR, and the NMEA decoding displayed information correctly. However, for some reason, it suddenly stopped working. When I used the UART tool to read the data, it appeared as Garbled code. How can I resolve this issue?

  2. iverson3ya_0-1694571394749.png

  3. Due to the problem mentioned in the first point, I decided to reflash the device, but I encountered a 'sync error' and couldn't flash it.

  4. iverson3ya_1-1694571553602.png

I would appreciate your help with the above two issues. Thank you.

4 REPLIES 4
Issamos
Lead II

Hello @iverson3ya 

I suggest you:

For the 1st part to follow these steps:

Screenshot_2023-09-13-07-59-14-50_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

Screenshot_2023-09-13-07-58-47-37_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

 for the second, you should follow those steps:

Screenshot_2023-09-13-07-58-16-15_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

Best regards.

II

I have followed these steps to burn the disc, but it still shows a 'sync error'.

Francesco Virlinzi
ST Employee

Hi

I see you were installing a new firmware.

Could I ask which firmware and which patch (scenario) you were installing?

I think you installed some 'RTCM based scenario' and now the STA8100 is senting RTCM (binary) data.

Regards

 Francesco

Try following these steps:

  1. On the board push and maintain the left (BOOT) white bottom
  2. On the board push and release the right (Reset) white bottom
  3. On Teseo-Suite - T5 Xloader panel - Push 'Start' button

Regards

 Francesco