cancel
Showing results for 
Search instead for 
Did you mean: 

PPS output from Teseo-LIV3R

hjsteger0
Associate II

What is the timing specification of the PPS (Pulse Per Second) output from the Teseo-LIV3R in terms of pulse width and/or duty cycle?  I've reviewed the datasheet, UM2523 (ST Teseo III ROM binary image - User manual), and UM2231 (Teseo-LIV3 GNSS Modules - Hardware Manual) but don't see this specified.

5 REPLIES 5

There are parameters and settings you can read out.

For the docs looks to be 1 Hz 50/50 duty, quantization probably +/-16ns

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
hjsteger0
Associate II

Hi Tesla DeLorean,

Thanks for the replying to my question.  In which document did you find this information?

Hi Tesla DeLorean,

I'm not sure if you saw my question from last week.  You wrote "For the docs looks to be 1 Hz 50/50 duty, quantization probably +/-16ns" but I can't find the document that specifies this.  Would you please tell me where you found this specification?

Sincerely,

Hal

TimBrookline
Associate

Additional question, is it the rising edge or the falling edge that is synchronized to the second rollover?

Hi,

For timing applications, I would consider using Teseo LIV3FL.

You can adjust the pulse duration (time from rising to falling edge) of the PPS signal by changing CDB-301.

Datasheet https://www.st.com/resource/en/datasheet/teseo-liv3fl.pdf

You can find the link to Software manual here.

https://www.st.com/resource/en/user_manual/um2229-teseoliv3-gnss-module--software-manual-stmicroelectronics.pdf

LIV3FL has same pinout of LIV3R but LIV3FL can do 3 constellations and is a flash based device.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.