2019-01-27 10:03 PM
Hi everyone,
I have designed a module with STA 8089GA which works properly. It gives me the exact position and fixes in less that a minute. I wanted to read time with this module. When I tried "PSTMGETRTCTIME" and "PSTMRTCTIME", it gives me time based on Greenwich. But I want the time based on the zone I live. I wonder how can I get the time based on the zone I live? Or generally is it possible?
I appreciate any help in advance
Best Regards
Armin
2019-01-28 12:10 AM
Time zones and daylight savings protocols tend to fall along geopolitical boundaries, you'd need to map those to make a determination of the adjustment necessary, or hard code a simpler value.
2019-01-28 12:27 AM
Thanks for your response, but, unfortunately I didn't got what you mean.
2019-01-28 1:01 AM
I think you can calculate it base on the longitude where you live, say GMT + x, and +1 (or -1?) for daylight saving, but for some country, the time is universal no matter the time zone you are in, so it is also based on the political consideration of that country. I think that's the reason why @Community member suggest hard code a simpler value.