Subject | Author | Posted | |
---|---|---|---|
Hello everyone, we currently devolping an Class D amplifier with the sta309a as DSP and TAS5624A f...
| 2019-06-06 05:07 AM | ||
When I am changing the number of channels to 1 channel. it is recognized by the windows driver, ...
| 2019-05-30 12:19 AM | ||
Good day! I want to use STA309A. I want to signal MCLK (XTI) 256*Fs, bicki to signal 64*Fs. Wh...
| 2019-05-02 01:10 AM | ||
Hello, hopefully this is the right place to post this. I am trying to use the Biquad Design Tool...
| 2019-04-26 11:52 AM | ||
How are you? I would like to test an ultrasound pulser IC evaluation board (STEVAL-IME012V1) on Wi...
| 2019-04-24 07:45 AM | ||
Battery Fuel Gauge via STM32. Whether provide test code?
| 2019-04-17 07:50 PM | ||
Hi, I'm writing a Linux audio driver for an Intel platform which requires an ACPI firmware node in ...
| 2019-04-08 02:59 AM | ||
2019-02-22 05:55 AM | |||
2019-02-19 02:24 AM | |||
Hello, I am using STA326 now and try to make mono setting. There is descrived the 1 Channel mo...
| 2019-01-23 06:30 AM | ||
I have built a circuit based on the tda7293 and it has burned instantly when connected. I have rev...
| 2019-01-14 06:00 AM | ||
HI, I am using ST mosfet (part NO STP28N65M2) in High input AC voltage limiting circuit (as per AN2...
| 2019-01-12 02:03 AM | ||
I HAVE USED IT IN A TEST CIRCUIT TO CHECK /VERIFY ITS SPECS. APPLIED VOLTAGE ACROSS ANODE/CATHODE ...
| 2019-01-07 02:43 AM | ||
2019-01-04 01:07 PM | |||
The datasheet of the TDA7294 audio amplifier suggests a bridge topology through Fig. 25 on page 13 ...
| 2018-12-28 04:57 AM | ||
Hi dear, I'm trying to set up an audio amplifier with quad half bridge STA515W. I've attached the ...
| 2018-11-24 02:30 PM | ||
Hi, We are planning to use STPM33TR in one of our switch gear product, this ADC has in built t...
| 2018-10-30 07:26 AM | ||
I want choose a part which has audio codec and audio amplifier in a single IC. It should support US...
| 2018-10-28 09:10 PM | ||
Hello! This is a manufacturer of PLC MODEM in Korea. My name is David Ko. Part number - TPL5010...
| 2018-10-12 04:03 PM | ||
I am using the STA350BW. While I tried to change the output gains by writing register 0x07, a nois...
| 2018-10-12 12:00 AM |