| Subject | Author | Posted | |
|---|---|---|---|
|
Hi We are currently working on a project using the nRF5340 MCU with Zephyr, and the interface betw...
| 2025-02-19 2:33 AM | ||
|
Dear ST/Forum, Preamble: We are using the LPS22HBTR pressure-temperature sensor in some PCB assem...
| 2025-02-05 4:58 AM | ||
|
I have a LIS3MDLTR connected over I2C on an aerial system that is used as part of our GNC system. ...
| 2025-01-29 6:25 AM | ||
|
Hi everyone, We are using the STEVAL-STWINKT1B board as a reference for the study of condition mon...
| 2025-01-16 12:12 AM | ||
|
We have an issue with LSM6DSM and LSM6DSV. Sometimes they start consuming abnormally high current o...
| 2025-01-06 12:04 PM | ||
|
HI When using the FIFO mode on the lsm6ds3tr-c sensor, there appears to be an issue where occasion...
| 2024-12-26 8:03 PM | ||
|
Hi Everyone, I'm using STM32L4 with LSM6DSM on IAR IDE and using motion AC library to calibrate th...
| 2024-11-29 5:22 AM | ||
|
Hello, We have implemented the LIS3DH with a nRF52832 in I2C mode on our board, and are using the ...
| 2024-11-27 12:18 PM | ||
|
Does the IIS2MDC require burn-in? Using the IIS2MDC, I read a magnetic filed of 0.47 Gauss on a Fri...
| 2024-11-12 8:20 AM | ||
|
I BOUGHT STEVAL- MKBOX PRO AND AM THINKING OF USING IT.
I have a wireless function, but pleas...
| 2024-11-10 6:57 PM | ||
|
After programming bluenrgm2sp module it is not discoverable in the ST BLE-scanner.I have used the b...
| 2024-10-27 10:39 PM | ||
|
I am using NRF5340 board for development using the LSM6DSO IMU sensor. Is there any way so that I ...
| 2024-10-26 8:52 PM | ||
|
Back in 2015, I ordered 19 LSM9DS0 boards from Adafruit for a project (which is taking longer tha...
| 2024-10-25 2:38 AM | ||
|
I have four sensor tile STWINKT1B kits. I want to simultaneously capture accelerometer, temperature...
| 2024-10-24 12:35 AM | ||
|
Hi Sir, What internal adjustments have been made to cause the noise density to differ between t...
| 2024-10-13 7:18 PM | ||
|
WE have got the Library from ST for nordic Cortex M33 Processor after signing the agreement, and tr...
| 2024-10-04 6:50 AM | ||
|
Hey,
I have been using the AIS2IH accelerometer senson in my TI's am652 linux based board. i fou...
| 2024-09-30 2:07 AM | ||
|
Hi, I am reading datasheet of LSM9DS1, and a little conccerned about the following part: ...
| 2024-09-25 5:33 AM | ||
|
Hello,
I have been working on a project using the H3LISD331Dl accelerometer set at +-400g and the...
| 2024-09-23 11:05 AM | ||
|
Hi. I'm an intern working with the SensorTile.Box Pro for a project. As the subject suggests, I wa...
| 2024-09-20 1:50 AM |