| Subject | Author | Posted | |
|---|---|---|---|
|
dear all, i want to recoed acceleration date from LSM6DSOX . i made app on st app and made output...
| 2025-07-23 9:15 AM | ||
|
Hi, I have a compulab SBC (UCMiMX8Mplus sbev) it is a dev kit. I am connecting the STEVAL-55GMB...
| 2025-07-17 7:48 AM | ||
|
I'm currently working with the LSM6DSV16X IMU and would like to connect an external sensor—specific...
| 2025-06-30 2:10 PM | ||
|
Hi, I am working on an accelerometer interrupt using the LSM6DSM. In AN4987 I found that I can con...
| 2025-06-27 12:23 AM | ||
|
I need to implement the clock wise motion using the sensor like LIS3DH accelerometer with i2c prot...
| 2025-06-24 4:33 AM | ||
|
I have implemented 9D orientation calculation on the STM32L4 using the LSM6DSO16IS and LIS2MDL sens...
| 2025-06-12 6:14 AM | ||
|
Hi everyone, I have set up my LIS2DW12 to recognise double taps in the Z direction, which works we...
| 2025-06-04 7:24 AM | ||
|
Hello everyone, I am using the LIS2MDL sensor in a parking project, where it operates via interrup...
| 2025-05-23 7:07 AM | ||
|
Hi, First of all, I'm not proficient with embedded C, but I would appreciate any input from you...
| 2025-05-19 10:36 PM | ||
|
Hello STM32 Community, I'm working with the LSM303AGR magnetometer/accelerometer sensor on an S...
| 2025-05-11 9:40 PM | ||
|
We've implemented an example program based on UM2220 using an lsm6dsox IMU sensor on an STM32U575 m...
| 2025-05-08 8:07 AM | ||
|
Has anyone tested the LIS2DE12TR accelerometer using lower input capacitance? I am interested in tr...
| 2025-04-30 11:27 AM | ||
|
Hi ST Community, I’m trying to use the LSM6DSO32XTR in Mode 2 (SensorHub) to stream data from two ...
| 2025-04-28 2:07 AM | ||
|
We are interfacing the IMP34DT05TR microphone with the STM32F423ZHJ6 microcontroller. I have attach...
| 2025-03-26 11:38 PM | ||
|
Hello friends; I aim to develop FreeRTOS STM32 based flight control card software. First of all, I...
| 2025-03-23 4:24 AM | ||
|
It seems that its CS is inactive, the LIS will assume that it should be in I2C mode. But if I have...
| 2025-03-12 11:14 AM | ||
|
Hello, I'm looking for any available douments/application notes on how to mount the sensor on a de...
| 2025-03-12 6:30 AM | ||
|
We have a ILPS22QS pressure sensor. We are getting an occasional i2c error. On investigation it s...
| 2025-03-12 12:45 AM | ||
|
I have an LSM6DSV16X configured to generate an interrupt on INT1 whenever the FIFO contains more el...
| 2025-02-25 5:58 AM | ||
|
Issue with Wrist Tilt Direction Detection on LSM6DS3TR-C Hardware & Software Details: - Sensor: L...
| 2025-02-23 10:52 PM |