Subject | Author | Posted | |
---|---|---|---|
Hello, I am using an Nucleo - F401RE MCU, with the CCA02M1 module, and the STEVAL-MKI155V1 microp...
| 2018-10-03 06:20 AM | ||
2018-09-27 03:48 AM | |||
In regards to the AIS3624DQ, I have a few questions about the part: Page 31 of the Data Sheet, pa...
| 2018-09-24 06:23 AM | ||
Hi, I have Using SPI Communication for interfacing AFE4300 sensor with STM32f4 board. I have devel...
| 2018-09-20 04:27 AM | ||
Hello. I am building a project using a digital microphone output. I will be giving the output of ...
| 2018-09-18 05:39 AM | ||
Hello everyone, I started with the implementation of the rotated ellipsoid fitting described in ...
| 2018-09-17 09:32 AM | ||
I am interfacing a LIS3DSH using SPI. My MCU is a Texas Instruments MSP432. When writing and che...
| 2018-09-13 04:25 PM | ||
Hello everyone, How does MEMS measurement ranges realized in hardware in details? Does it use:...
| 2018-09-13 12:01 PM | ||
im using the feather nrf52832 with the featherwing. i can read the ID by sending 0x00 as [0x80,0x8...
| 2018-09-13 12:13 AM | ||
Since there's no information on the registers in the datasheet, and half of the API is in the docum...
| 2018-09-12 12:13 PM | ||
2018-09-12 06:11 AM | |||
Trying to run Echo Cancellation Demo using X-NUCLEO-CCA01M1 , X-NUCLEO-CCA02M1 and NUCLEO-F446RE wi...
| 2018-09-10 01:07 PM | ||
Hi, By default the temp, humidity and pressure are enabled in the end node example and i would lik...
| 2018-09-06 02:18 AM | ||
Our customer is looking for high-rate magnetic field sensing, with a soft target of 100 kHz. Is thi...
| 2018-08-29 10:41 AM | ||
Hello sir Greetings !!!!! We have selected your TOF Sensor part number vl5l0x this sensor det...
| 2018-08-29 06:00 AM | ||
When I first boot the board the accelerometer is not recognized in IIO. After a reboot it does or i...
| 2018-08-23 05:02 AM | ||
Hi! I have a custom pcb with Lsm6dsl connect to mcu (nrf52832) via i2c. I can write and read re...
| 2018-08-23 03:21 AM | ||
2018-08-21 12:05 PM | |||
I try to add mutex in the X-CUBE-53L1A1 SimpleRangingExamples I have defined #define VL53L1_Get...
| 2018-08-21 06:51 AM | ||
2018-08-18 06:41 AM |