Subject | Author | Posted | |
---|---|---|---|
2020-07-20 10:30 PM | |||
2020-07-16 10:10 PM | |||
I am using VL53l0x and I want to measure distances of 2 meters but I don't find the function to con...
| 2020-07-15 03:35 AM | ||
VL53L1_GetRangingMeasurementData() ONLY returns data[0] buffer as result. It means that I will get ...
| 2020-07-02 01:15 AM | ||
I'm using the lsm9ds1 as part of a bought module - the arduino nano 33 ble - which can achieve very...
| 2020-07-01 03:00 PM | ||
Hi, my name is Vincenzo. I would like to: perform the 3 calibrations ( RefSPAD, XTalk and Offs...
| 2020-07-01 12:36 AM | ||
I have been experimenting with the X-NUCLEO-53L3A2 and have grabbed some quick measurements to see ...
| 2020-06-29 10:02 AM | ||
I am working on a project/proof of concept that requires measuring the distance to a person relativ...
| 2020-06-23 10:24 AM | ||
When the LIS2DW12 is asked for the first time for ID it does not response(responses with 0xFF). Th...
| 2020-06-16 05:15 AM | ||
While implementing the middleware for vl53l0x I am facing the following problem. Can you please let...
| 2020-06-10 02:39 PM | ||
In the docu's of VL53L3CX I couldn't find the size of SPAD array. For VL53L1X it was 16x16 pixels, ...
| 2020-06-05 06:34 AM | ||
I'm using the evaluation board, that is provided with two type of transparent windows. Is possible ...
| 2020-06-05 02:12 AM | ||
I use Arduino Uno and VL53L0 sensor appliction board. I measure a distance long time. (8h or more)...
| 2020-06-03 11:57 PM | ||
Hello, I have multiple VL6180X sensors which are handled by i2c multiplexor. Once I power up the s...
| 2020-06-01 06:07 AM | ||
Hi, I try to read the VL53L0X sensor using the continuous read function. When I try to read the ...
| 2020-05-27 01:17 AM | ||
2020-05-20 06:32 AM | |||
I am measuring on black targets from two differnent distances. 34mm (real target distance) with ...
| 2020-05-20 02:51 AM | ||
2020-05-04 11:22 PM | |||
2020-05-02 04:40 PM | |||
If it's not completely transparent ice but translucent ice, can you pass?
| 2020-04-18 03:15 AM |